Hello all
I am having trouble with the reliability of my design using the LM5105 as a solar charger (see attached circuit for reference).
In an earlier prototype board I had inadvertently inserted a series resistor between HO and LO and their respective FET’s gates and guessed a value of 10 Ohms, my logic at the time was to limit the inrush currents to the FETs. This worked well (well enough for the time I had) but reading through the specs I could see no reason to have them, it was better from a power management point of view to have the FETS turn on as fast as possible thus managing the heat dissipation within the FET’s, so I had them removed. Bad move..! With this configuration the design would fail regularly, only lasting a matter of weeks. Typical failures would be the LM5105 and the low side FET, I am not sure which device failed the other. The frustrating thing is the device works well as a solar charger but I have boards that have run for a few months and I have boards that fail almost immediately. The devices is hardly being put through its paces as the size of the panel used so far are only10W. (I have designed it to be able to deliver 4.5 A and I know it ‘capable of delivering those currents)
Out of desperation I have reinserted the10 Ohm series resistor to see if things improved and they have but not completely. Can anyone explain why this is so. According the specs, the LM5105 is capable of delivering the currents to drive the two FET’s, what I am seeing here are the two series resistors absorbing some of the power delivered by the LM5105 protecting it from its inability to deal with its own power dissipation. The FET’s used are also low ERS FET’s as per the recommendations. I have followed the recommendations for the pcb layout and have kept the tracks as short as possible. If the low side FET is failing the LM5105 why..??
The 10 Ohm resistor, is as I have said was a guess, would a 15 Ohm be better? I have scoured the web for application notes on this device but there is little information about. If anyone could shed some light it would be very much appreciated
Cheers
Ant