Isolated power experts,
I have a customer that is worried that their Minimum OVP from HVSEN on the UCC28061 will be lower than their highest regulated voltage. We may need to have a test engineer look at their past data here to confirm the corner cases and if they happen at the same time. The customer's question is :
Can the Vref be all the way at 6.18V and the HVSEN OVP be all the way at 4.64V at the same time?
(those numbers are based on max Vref and min HVSEN rising OVP over temp)
Some background:
"Here is the problem. We use 1% tolerance resistors to set the PFC DC Bus voltage to 403VDC, we pick 403VDC to get good holdup time. We use a 450VDC rated alum elect cap. We set the OVP voltage to 447VDC also using 1% resistors. The 450V cap has a surge rating of 500VDC.
With worst case stackup of tolerances, the highest regulated voltage is 421VDC and the lowest OVP voltage is 418VDC. This means that if all the tolerances stack up in the wrong direction the UCC28061 with constantly be in OVP."8080.UCC28061 PFC Bus Voltage tolerance.xlsx
I've tried to attach the customer's excel calculation spreadsheet to show how they are determining this.(Let me know if it is not attached properly.) If you all can comment if this looks correct that would be beneficial as well.
Thank you,
John Stevens