Hy, i must use an LM2576HVT-ADJ (Flow LB03), for regulate an output light, I want use the pin 5 (ON\ OFF) for regulate the current in output.
Like this i must switch very fast this PIN with a comparator and a shunt, i have a fixed 24 Volt in output but when the current reach a value i cut-off the pin 5, here the pin 5 is in continuos fast switch on/off... IS POSSIBLE USE THIS APPLICATION, OR THE LM2576 DAMAGE OR NOT REGULATE THE OUTPUT COSTANT?? THANK YOU VERY MUCH ]