This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using the IC BQ24600 for charging the 14.8V,11Ah battery.In the board all voltage level seems ok but
Vout is 0.8V. There is no waveform at HIDRV & LODRV. Led SAT is blinking and /PG is cont. glowing.At TS Pin
voltage is 1.6V,VREF,CE is 3.24 V. ISET pin is 0.6V. REGN pin is 6V, and the bootstrap capacitor is 4.62V.
plz clarify....
Thnks
ASHOK
I got the answer.....full batch of the IC is bad....i replaced by sample and now its working fine..
thanks to all
Dear all,
do you have further information about weather there is a bad batch?
I'm about to go into production so tis is important.
thanks.
I have not heard of a bad batch. There are clones to ICs out in the market. Make sure you but parts from a reputable distributor.