This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Inquiry regarding TPS84259 RRT value setting

Other Parts Discussed in Thread: TPS84259

Hello, all

Now we are evaluating TPS84259 for our new design, then would like to know regarding RRT value settings on this device.

We understand that this device could adjust the switching frequency in accordance with the value of RRT. However, we could not find actual equation on excel calculator.

(We are not willing to use external oscillator to set switching frequency, but to use RRT resister.)

Also, please refer to enclosed excel file, which contains actual input/output condition on this device.

We thank you in advance for your information.

Best regards,

1777.TPS84259 Calculator ver 1.0_2.xlsx

  • It is recommended to operate the TPS84259 at a switching frequency of 800kHz. An Rrt value of 0Ω sets the switching frequency to 800kHz. Only in applications with both an input voltage greater then 18V and an output voltage between -3V and -8V is it recommended to reduce the switching frequency to 500kHz.

    This information can be found on page 18 of the datasheet.