All,
I bought UCD3138HSFB EVM and try to download code into EVM, we found the error as attached. 2112.Presentation1.pptx
-Open Device GUI(Version 1.8.325)
-Scan device in ROM mode, the GUI say "no ROM detect"
I notice that no LED indicate on EVM board(USB to GPIO should be OK as It's green LED )and not sure the EVM is ready to download the code? or I miss something on the EVM board.
Thanks.
NT
anyone