This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210 External clock

Other Parts Discussed in Thread: TPS40210

Please look an attached file.

I input a direct clock into RC without FET, and may the external synchronize?

Why are FET Rrc and Crc necessary, when TPS40210 is external synchronization?

TPS40210 External clock.pdf
  • The RT function inside the TPS40210 is not a PLL.  It is a simple timing system that uses an external R and C that charges from then input voltage.  There is an internal switch that discharges the capacitor.  The external clock function shown is just an open drain that is used to discharge the the timing capacitor externally.  It must be operated at a higher frequency.  it may be possible to construct some other direct drive scheme, but the datasheet operation looks to be the simplest.