This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lm25101 bootstrap capacitor

Hello,

I plan to use an LM25101A gate driver in a Buckconverter application.

Is the value RD on page 5 in the data sheet to understand like a series resistor with the Bootstrap diode? Are there any min and max values for the bootstrap capacitor? I have 44V on the buckconverter input, 14V on the output and 14V as VDD for the driver. I am using infineon BSC039 MOSFETs with a total Gate chate of 32nC.

Thanks for you reply

Markus