This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3432B - Problems (no current regulation, no control, no PWM) for LCD Back light Control

Trying to use the LM3432B to control LCD back light using 5 sink pins (all but IOUT6) @ 20ma each.  R(iref) is 54.9K (should be 5x20ma).  Iout6 is grounded.  Iout1-5 are all tied together and "sink" the back light.  Mode, Agnd, Pgnd, and Thermal_Pad pins are all grounded.  Cvcc has a 1uF ceramic cap (not tied to anything else).  Cvin also has a 1uF ceramic cap.

Vin is +12VDC (through a pull-up resistor that I have varied from about 20 to 70 ohms as I have tried solutions).  The back light voltage is specified as 4 to 4.4 VDC at the nominal operating current of 100 mA.

Initially I tied the Vin and the anode of the back light together pulled up to the 12VDC through the resistor just described.  I soon realized that I was forcing the chip to regulate the current in the back light at a Vin that was less than 6 volts (remember the Vlcd is about 4.2 volts) and the internal regulator (Vcc) was not working (the input was less than 6V).

By adding either a resistor (10 or 20 ohms) in line with the back light OR a zener diode (about 2.4 volts) I was able to "break" the connection between Vin and the Vlcd which allowed the internal regulator to have 6+ volts (the Vlcd plus the voltage drop across the resistor OR the zener).  The part that I don't understand is that the voltage at the Iout1 to 5 pins (still tied together to the cathode of the back light) is always very small (<.02 volts) and I would expect it to be higher if the chip was actually regulating the current.  I don't know why.

My conclusion is that it is NOT regulating the current for some reason even though the internal regulator seems to be working (Vcc = 4.9 volts).  In addition NEITHER the enable OR the DIM inputs have any effect on the operation of the circuit (another clue?).  I can see the enable pin input changing from Off to On and the chip ignores it (back light is always on).

I realize I am probably doing something "stupid", but have not been able to figure it out yet.  Any help or clues would be appreciated.  I think the PWM circuit is probably not working because our PWM frequency is pretty slow.  Regardless I can't understand why the enable pin is not working.