This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Start-Up Question of LM22672/LM22680

Other Parts Discussed in Thread: LM22680, LM22672

Hi~

Out customer use LM22672/LM22680 device.

But Our customer have start-up problem.

* Condition :

- Vin : 10V, Vout : 7.1V

- Current : Nominal(Under 30mA : Non operating Motor), Active(1A, Operating Motor)

* Status :

 - Start-up current is abnormal(Condition : Vin=10V, Vout=7.1V)

 - Start-up current is normal(Condition : Vin=11V, Vout=7.1V)

In Light load condition, Do i need minimum gap of the Vin and Vout??? 

But Our customer can't change Vin level.

If see attached file, You can know status(I attached Measurement graph/ schematic and so on)

Our customer don't have many time. Please reply to me as soon as possible.

LM22672_LM22680 Question.doc