This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS57114-Q1 fpmod calculation.

Other Parts Discussed in Thread: TPS57114-Q1

Dear support member,
About TPS57114-Q1 fpmod calculation.


Iout=4A、Vout=1.8V、Cout=44μF
Calculated taking into equation (36)is  fp mod=8.03kHz.
Could you teach the reason why is not fp mod= 6.03kHz?

Could you check the attached file?

Regard.

Bob Lee

8463.TPS57114-Q1_fpmod calculation_140424.pdf