This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61220 With Dimming feature

Other Parts Discussed in Thread: TLV61220, TPS61070, TPS61200

Hello Team,

one of my customer wants to add the Dimming feature in a Led lighting application where TLV61220 is used.

can you please help to know how we can add the analog dimming feature here ... the basic specs are as below ... 

Specs :

  • Battery Ratings & Chemistry : : 2.4V, 1200mAH &  Rechargeable Ni mH
  • System O/P : 3v - 3.2v @ 160mAmp
  • Load Rating : 0.5w Single Led
  • Features : Analog Two stage Dimming (using Switch)
  • Dimming Ratings : 1st Dim @ 70% (120mA) & 2nd Dim @ 50%(80mA)

Attached is the concept design used for non dimming requirement earlier. 

We are thinking on Op-Amp (LM35x) approach but unable to get the results ...can you please let me know how to add dimming here.3124.7418.0.25w Study Lamp.pdf