Good evening.
I am designing a solar power supply that needs to generate outputs for two different loads over a 24 hour period. The MCU load @3.3V is approx as follows:
- 8mA continuous
- 80mA for 20mS 720 times a day
- 250mA for 15mS 720 times a day
The main load current @3.3V requirements are quite high at approx:
- 16A for 5mS 48 times a day
- 7A for 50mS 48 times a day
Detailed load analysis reveals the circuit requires ~0.2Ah per day to keep the system operating so for my preliminary design I selected the BQ25504 coupled with a MS-M5050 solar cell and 1100mAh LiFePo4 battery.
The spec sheet of the BQ25504 states the load is to be connected to VSTOR but I'm not sure the IC could handle the peak current requirements of the main load let alone the MCU.
So my questions are:
- Is the solar cell a good match for the BQ25504? Is there a list of recommended solar cells for this IC?
- Can I connect both the MCU and main load directly to VBAT? What are the pros/cons of this config?
- Can I connect the MCU to VSTOR and main load directly to VBAT? What are the pros/cons of this config?
- Can the BQ25504 handle the current requirements of the MCU if connected to VSTOR?
- What sort of loads can be successfully connected to VSTOR?
- Is there a better MPPT IC choice given the unusual current requirements?
Thanks in advance,
Franc