This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910 Power Sequence

Other Parts Discussed in Thread: TPS65910, AM3352

Dear all.

Our customer evaluate the TPS65910 for AM3352.
1) When VCC7 has not reached the voltage which outputs 3.3V of VDD2, is the Power control state-machine waiting for execution of a sequence?

2) When VCC7 is less than the voltage which outputs VDD2, is there any situation where VDD2 is not outputted and reset is not assert?
    The VCC7 voltage returns again and VDD2 is output.

Regards,
PAN-M