Hi,
I have a question about Boost design.
I want to use +12V input to get +48V/1.5A output. Can it be done by LM5000? If output can't be up to 1.5A then what is max?
Thanks.
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kevin,
The peak current requirement of your application exceeds the capability of LM5000. LM5000 has 1.35A min (2A typical) switch current limit, and 1.35 A min should be used for worse case.
Assuming 30% peak to peak current ripple and 90% efficiency, the required peak switch current of your application will be 48*1.5/(0.9*0.85*12)=7.8A, which is way higher than 1.35 peak current limit of LM5000.
We can put it in another way, the max output current LM5000 can support for 12V to 48V boost is around
12*1.35*0.9/(1.15*48)=0.26A.
I would recommend you to take a look at boost controllers LM5020 or LM5022.
Thanks.
Haifeng