This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMIC TPS61091

Other Parts Discussed in Thread: TPS61091

Hi TI,

                   I m using PMIC TPS61091 Boost  Converter and i selected this because exactly i need 3.3V at output at 500 mA with Low battery indicator as per Requirement of my project. I have connected the PMIC as referred in the datasheet .But the output which i m getting is 4.74 V or 5V. i would like to know the output Adjustible Resistors values . In my System i have given 1M ohm and 200k ohm at ouput side.

                                                     since it is a fixed Version 3.3V output PMIC IC , i also Removed above resistors and tested but i dint get the results...     Please assist me.