This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Iout ripple of TPS92640

Other Parts Discussed in Thread: TPS92640

Dear All,

Would you tell us how to use TPS92640?

When our customer operated TPS92640 at the following conditions,
they confirmed that a Iout's ripple occurred on their board.
Vin:12V
Vout:6V
Iout:0.8A
I attach a customer's circuit diagram and the  waveform of the output current.

Our requests are following.
・Is there the abnormal point on the customer's  circuit?
・Please give us a recommended circuit diagram at the situation of Vin12V、Vout6V、Iout2A.
・When customer uses TPS92640, is it necessary  that they add slope compensation circuit to their board In the situation  of more than Duty 50%?
・Please give us the opinion of the likely cause that the Iout ripple occurred.

Best Regards,
Tsuguhiko Asai

Customer's Circuit and Waveform of Iout.pdf