I want to teach the questions.
We test under the following conditions
But output voltage is dropout.(12Vout→5Vout)
1.Output possible? Under the following conditions:
Vin 12.5V
Vout12V±10%
Iout:(min)0A/(typ)0.53A/(max)/2.51A
2.If No.1 question is possible. Please teach us recommend peripheral circuits..
【TPS40060EVM use
Ch1:Setting Vin12.5V→Vout12VIout0A
Ch2:Measured value Vin12.5V Vout12V Iout0A
Ch3:Switching Waveform】
【TPS40060EVM use
Ch1:Setting Vin12.5V→Vout12VIout0.53A
Ch2:Measured value Vin12.5V Vout5V Iout0.53A
Ch3:Switching Waveform】
【TPS40060EVM use
Ch1:Setting Vin12.5V→Vout12VIout2.51A
Ch2:Measured value Vin12.5V Vout5V Iout2.51A
Ch3:Switching Waveform】