Hello, I just want to write a small program to be used for production programming the golden DFI file, instead using TI- Tools for this Task because the Tools are useful for developers but probably not designed to be used in production :-(, ok, as a starting point I've read SLUA504A (Going to production with the bq2754x), starting on Page 9 I've found a nice "howto"- flow chart, but how do I "read 96 bytes from data register ..." or "read register 0x66" ? I did not find any docs according to the ROM- Mode of the device ( I2C Adress 0x16), only "normal" read/writes to/from address 0xaa/0xab ?
So, my questions are:
1) does anybody at TI have a doc regarding the ROM- Mode of the BQ27541-G1 ( commands ? ) or if not applicable
2) what bytes should I send to perform "read register 0x66" ?
Thx for any help, best regards, Enrico
PS: It would be *very* nice if an TI- employee have an answer for me, or at least some hints where to look for some documents ;-) ....