How can I automatically shut down the TPS92512 when IADJ = 0 mV?
Assume I do not have the luxury of more than one output pin from my microcontroller, so I cannot use one pin for PWM and another pin dedicated for either UVLO or PDIM. The input to the IADJ pin must shut off the LEDs when the voltage is close to 0 mV.
Would a circuit like this work?
When IADJ is well above 0 V, the voltage at UVLO will be well above the threshold to keep the LED driver on. As IADJ approaches to 0 V then the voltage at UVLO will drop below the threshold voltage and the output will be shut off.
A more precise way to do this would be to use a comparator like the LM211 but this would add cost and space which would be worth it only if the tolerance on the shutdown threshold is tight.