Hi,
I got two questions about the reference design PMP10592.
- What’s the actual load current? The internal reference for average current limiting is 50 mV and the current sense resistor is 50mΩ on the board PMP10592, so the load current should be 1 A, correct?
2. What the function of the circuit shown in the red cycle? If it’s used.
Thanks a lot.
Best regards,
Jason