Hi,
I'm looking for some informations about bq34z100-g1.
How Can I update embbeded firmware of gauge ?
thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm looking for some informations about bq34z100-g1.
How Can I update embbeded firmware of gauge ?
thanks.
Tom,
Which is the communication interface used to upgrade firmware I2C or HDQ link ?
for me, firmware is the embedded soft put into the xemic's CPU Core
Serge,
Tom,
I'm working now with bq34z1xxEVM board
Gauge's has been updated with bq34z100-g1 firmware
I can read register, unsealed or send other command with bqStudio
Now my problem is how to define my battery's parameter. I have found how to set design capicity but not voltage capacity.
Another thing, When I'm trying to make a calibration, software return an error if voltage value is upper 7800 mV
for information, my battery type is NiMH, design voltage is 12000mV an design capacity 9000mAh.
Any Idea ? Thank for you help
Regards,
Serge
Serge,
You are correct, there is a typo and this is how it should read.
3.2.1 Cell Configuration
The bq34z100 operates in one of two modes for measuring battery voltage. Place two jumpers on header
J5 to select the mode of operation. Refer to the Section 2.3.
For packs where the stack voltage is less than 5 V:
• Set the Number of Series Cells parameter field to the appropriate value
• Reset the gauge using the RESET button on the Commands panel
• Calibrate the stack voltage. Reference the Calibration Screen section
For packs where the stack voltage is greater than 5 V:
• Set the Number of Series Cells parameter field to the appropriate value
• Set the VOLTSEL bit in the Pack Cfg A register
• Reset the gauge using the RESET button on the Commands panel
• Calibrate the stack voltage. Reference the Calibration Screen section
Thanks
Tom
Hi,
After calibration, I'm beginning to setting parameters for my batteries. When I'm reading bq34z100-G1 documentation (SLUSBZ5 - JANUARY 2015), I see that some gauge internals registers not documented (for example pb EFF Efficiency, Cell Taper Voltage, NiMH Delta Temp, ...etc.
Is there another documentation as user software manual which contains more informations and that can help to me to set internal register for NiMH and Lead Acid chemistry device.
Thanks
Serge