Hi
Abnormal waveform is I was able to confirm in TPS2393A of EVM.
VIN :45.5V
UVLO:45V
LOAD :78Ω(About 600mA)
COUT :386uF(100uF+68uF×2+150uF)
FAULTTIME:27nF
IRAMP :2200pF
When the input voltage is turned ON by at about UVLO,
It confirmed the abnormal waveform.
Please tell me , Is this normal operation?
Best Regard
T Kishi