Hi
We are using PTH04040 power module in one of our board for generating the 1V output from 5V input. We manufactured 10 boards with the power module. Out of 10 boards,in 5 boards the power module is not generating the output at all times.
In 5 boards,the module is generating the 1V output as desired after powering on the board . Measured voltage is 4.2V at INH (pin no: 7 ) and also 0.79V at VO-ADJ,Mar-Up and Mar-Down(Pin no: 17,19,20) in working module.
In Non working module, . measured the voltages as follows 4.2V at INH (pin no: 7 ) , 0.79V at Mar-Up( pin no:19) and 0V at VO-Adj ,Mar-Down(Pin no: 17,20) . Some times this non working module is generating the output if do powering on and off the board many times.
We have connected 36.5K with 0ohm series resistor between pin no:17 and ground to generate 1V output. Even ,I have removed the two series resistors and mounted 36.5K directly between pin no:17 & 18.
As per datasheet specification, the Voltage VO-ADJ should be in between 0.8V and 2.5V.
The input voltage 5V is fine at all times. Our current requirement is 35A.
Please find attached the Schematics
Need immediate suggestions to sort out the issue.
Thanks
Sakthi.APOWER-POLA-Schematics.pdf