This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Combining Multiple Switchers for high power DC-DC boost converter

Other Parts Discussed in Thread: LM5122

I used Webench to find a couple of reasonable solutions for this application, which is a high power communications amplifier.

DC Input Voltage = 28.0VDC

DC Output Voltage = 49.0VDC

Output Current = 25.5A DC

Max temperature = 65°C

Total output power 1250W, DC

I have a solution for ~10A using either TPS40210 or TPS43060 - both of which can drive a load up to 10A (although it seems the designs are actually capable of more), and I need to combine three of them for my ~26A requirement.

So my question is - is there a better way than combining three discrete DC-DC boost converters? I do have the board space for three of them, and $ wise its ok, although it would be nice to run three converters off a single controller?

I searched through reference designs, but the high power capable supplies are AC-DC designs and use a different topology.

So assuming, this is the best approach, then can I just combine the three of them? Do I need to drive them out of phase so the ripple does not add? What is a good strategy for this - is it enough to use a micro to stagger the sync line in the case of TPS43060?

Thanks!