Hi,
We are using BQ24195 for battery charging and power path management. When we plug in 5VDC 2A adapter or 5VDC 2A DC source, we are observing only 500mA. We are using USB cable to charge and the DP and DN are shorted to make it as DCP. As per my understanding DCP should draw up to 1.5A but not getting in our case. Battery voltage measured during this period is 3.7V
Register dump and schematics are attached for reference. ILIM resistor also changed to 330Ohms to set the fast charging current to 1.5A
Please refer the below attachments and advice on what could be wrong.
Thanks and Regards,
Nigil
bq24190 1-006b: bq24190_irq_handler_thread: ZZZZ Read all registers
bq24190 1-006b: bq24190_read: reg = 0x00 data = 0x35 0xd4
bq24190 1-006b: bq24190_read: reg = 0x01 data = 0x1b 0xd4
bq24190 1-006b: bq24190_read: reg = 0x02 data = 0x60 0xd4
bq24190 1-006b: bq24190_read: reg = 0x03 data = 0x11 0xd4
bq24190 1-006b: bq24190_read: reg = 0x04 data = 0xb2 0xd4
bq24190 1-006b: bq24190_read: reg = 0x05 data = 0x8a 0xd4
bq24190 1-006b: bq24190_read: reg = 0x06 data = 0x03 0xd4
bq24190 1-006b: bq24190_read: reg = 0x07 data = 0x4b 0xd4
bq24190 1-006b: bq24190_read: reg = 0x08 data = 0xac 0xd4
bq24190 1-006b: bq24190_read: reg = 0x09 data = 0x00 0xd4
bq24190 1-006b: bq24190_read: reg = 0x0a data = 0x23 0xd4
bq24190 1-006b: bq24190_read: reg = 0x08 data = 0xac 0xd4
bq24190 1-006b: bq24190_charger_get_online: online = 1
bq24190 1-006b: bq24190_read: reg = 0x09 data = 0x00 0xd4
bq24190 1-006b: bq24190_charger_get_health: health = 1
bq24190 1-006b: bq24190_read: reg = 0x08 data = 0xac 0xd1
bq24190 1-006b: bq24190_charger_get_online: online = 1
ltc cap[3289600][65535]
bq24190 1-006b: bq24190_read: reg = 0x08 data = 0xac 0xd0
bq24190 1-006b: bq24190_charger_get_online: online = 1
init: untracked pid 3165 exited