1. Need to design bq24650 for 10A charge current.
Input is solar panel connected.
2. Looking at schemtic of evm I am making following changes:
Lo = 3.3uH
Co = 40uF
Sense = 10mohm
Mosfets: 2 in parallel
3. is there anything else to change? I have connected two mosfet in parallel due to high current.