I'm noticing a different behaviour between two runs of a design based on the BQ24133 battery charger. In both situations the batteries seem to charge fine. I want to be sure that I know what the proper behaviour should be. I am using it to charge a 2cell 8.4V Li-ion battery.
On an earlier run, when the battery is connected and then the unit power on VBAT would be the 2cell voltage and it would charge normally. However, on this run the voltage level seems to be the current voltage of the battery + 0.5V until it reaches the 2cell voltage level.
I noticed some charging information in the post below showing the typical charging profile. In the fast charging phase the charge current should be constant with the voltage of the battery increasing until it's charged. This seems to suggest that I should be seeing the battery voltage increase at a steady pace until it's reached a threshold where the charging current exponentially decreases.
https://e2e.ti.com/support/power_management/battery_management/f/179/t/359600
For the current configuration, I have Ichg set to 2A by using a 100k-13.7k voltage divider using the VREF pin. For RSR I'm using 10m Ohm value used in the datasheet. For ACSET I'm using a 100k-57.6k voltage divider and a 20m Ohm sense resistor across ACN and ACP like the reference in the datasheet.
What waveform should I expect VBAT to follow as it charges? Should it immediately be 8.4V while connected or should the voltage across the battery gradually increase over time? Is one waveform representative of precharge and the other fast charge?