Hello,
I have two questions about UCC28070-Q1.
I attach a file.
A_4-phase_90-degree_20151001.pptx
Regards,
Daisuke
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have two questions about UCC28070-Q1.
I attach a file.
A_4-phase_90-degree_20151001.pptx
Regards,
Daisuke
Hello John,
Thank you for your reply.
When the ON-DUTY is 50%, the phase-shifting is not 90° but 180°.
Please teach me the reason.
I attach a file.
PFC_4-phase_phase-shiting.pptx
The conditions are as follows.
(1)SS-pin Output impedance is 1/2. Line is common with two ICs.
Past:Css=3.2uF
Now: Css=6.4uF
(2)VAO-pin Output impedance is 1/2. Line is common with two ICs.
Past:Cpv=0.33uF, Czv=3.2uF, Rzv=43kohm
Now: Cpv=0.66uF, Czv=6.6uF, Rzv=22kohm
(3)Rimo-pin Output impedance is 1/2. Line is common with two ICs.
Past:Rimo=43kohm
Now: Rimo=22kohm
(4)Vsense Line is common with two ICs.
(5)Vinac Line is common with two ICs.
(6)PKLMT Line is common with two ICs.
(7)CDR-pin snd Vref-pin is shorted. Ccdr is the same in the past.
(8)Rrt Calculated by equation-8.
(9)Rdmax Calculated by equation-4. Satisfying equation-10.
Past is 2-phase. Now is 4-phase.
Best regards,
Daisuke
Hi Daisuke
The waveforms you attached show the inductor currents.
You should look at the gate drive signals and you will find that the gate drives have the correct phase relationship.
Regards,
John
Hello John,
Thank you for your reply.
I ask customer to check the gate drive signals.
And,
Could you please check the circuit parameter described above(1~9)?
Please teach me problems if there are problems.
Best regards,
Daisuke