Hi Chris,
I found following thread that discussed about switching frequency of TPS62085.
Now I also found this behavior on EVM, but I can't find such behavior from information in datasheet. From fig.1 in datasheet, I assumed that it should be 2.4MHz at 3A load but it was approx. 1.4MHz with 3.3V input. On the other hand I can see 2.4MHz with 5.0V input. So please explain the mechanism of this switching frequency variation.
Please refer the waveform at 3.3V and 5.0V input I measured.
TPS62085EVM Switching Frequency_20151104.pdf
Best Regards,
Sonoki / Japan Disty