We are seeing some significant overshoot and ringing on the VPOS output of a 65130 regulator. Power save mode is selected and when the burst regulation occurs we see a 0.8 volt overshoot and ringing. This is very problematic as the +/-15V supplies are used for an audio amp.
Even though we have the same connections for the -15V output we are not seeing the same thing with it.
Can you help us figure out how to eliminate this massive noise problem? Circuit and scope output of +15V attached.
Load for both +15 and -15 supplies are only about 40mA.