I'm using a TPS54240 device in a DC/DC converter application. In 2 out of 50 units I have seen a shutdown of the TPS54240 after operating for "a while". The converter design is not near the performance limitations of the part:
24 volts input
5 volts output at ~400 mA output current
One of the parts that failed will operate properly when initially powered, and will shut down after prolonged operation (~2 hours). The part will not function upon power cycling. It will operate after resting for > 1 hour.
The other failed part functioned intermittently when initially powered on. After running for ~4 hours, the part shut down and will no longer operate. Neither part draws excess current when in "shutdown". Die temperature does not exceed 40 C. At my load, I would not expect a thermal shutdown until ambient temperature in excess of 140 C, based on the calculation in section 8.2.1.2.12 of the TPS54240 data sheet (page 37). Is there another mode of failure I should be looking at other than a thermal one?
Thanks,
Cliff