Hi Sir,
I have a TPS40400 design. The processor is DM8168. I want to change FREQUENCY_SWITCH(33h) and MFR_SPECIFIC_00(D0h). So, I use the processor’s I2C interface to change these registers. But it doesn’t works. Our I2C command can read these registers correctly. So, I am not sure if any register needs to be set first so that I can change FREQUENCY_SWITCH(33h) and MFR_SPECIFIC_00(D0h).