This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have some trouble getting the LM3405A to work properly - I'm using the circuit and recommended parts from page 18 on the data sheet. Vin=5V driving a single LED @ 1A I do not get 1A current instead I get
R: 0.61A
G: 0.32A
B: 0.4A
W: 0.38A
The output current is dependent on the forward voltage of the LED and not even close to 1A. I tried changing various components e.g. L1 to 6.8uH, D2 to BAT54, I also verified that R1 is indeed 0.2R. Increasing Vin to about 6.6V brings the current up to the correct range. I'm attaching the PCB I'm using - any feedback is greatly appreciated.
The EN/DIM is tied to 5V - Using PWM input works as well just not at the correct Imax. I'm using a Cree XML RGBW (single color/per driver). The Vtyp are R:2.2V/G:3.3V/B:3,1V/W:3.1 V. This is already the second board I made following the PCB recommendations in the data sheet. I first one showed the same problem but with currents even smaller. Let me try to make scope shots tonight ...
Thanks.
I remeasured - the voltage at the PCB was indeed a little lower - so I adjusted the power supply that I have now exact 5.0 at the PCB Vin pin. Instead of using an DMM anywhere in the LED path I used now the power supply current reading which is @0.68A - frequency at the SW pin did not change. Cranking up the voltage at the PCB to 5.8 V will give me 0.93A but >5.8 it breaks down. Voltage at the L- pin on the PCB is 0.233 and at the L+ pin 4.41V. At the green LED it's 3.96/0.78. The leads are about 39 inches long as seen on the image. Measurements are done with a Fluke 73III.