This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I want to use the LM3405A as a constant current driver for NiMH cells. In my configuration, I have 2 NiMH cells, and a BQ2002E that regulates the battery charge profile. I want to charge the batteries at 800mA and my lowest possible Vin is 4.2-4.5V. The NiMH voltage ranges from 1.8V-3.2V during charge and spends the majority of the charge cycle between 2.8-2.9V.
Summary:
Icharge = 800mA
Vin = 4.2V - 4.8V
Vload = 1.8V - 3.2V (the majority of the time between 2.8V - 2.9V)
BQ2002E configured for a 2xNiMH charge controller
I have an Eval board for the LM305A. Questions:
1. Is it possible to use the LM3405A in this configuration?
2. I understand that I have to change R1 to 0.25 ohms for 800mA. What other optimization should be done?
Regards,
...kevin
Hello Kevin,
If you need a constant current source then an LED driver is a good option, that is what they are set up for. The LM3405A should work well for you.
As for other optimizations that kind of depends. But it's a relatively simple circuit so your main concern may be the current ripple, although the charger PSRR may compensate for that. So really just follow the datasheet regarding input/output capacitor and inductor selection and you should be fine. If you have particular concerns let me know and I can probably help.
Regards,
Clint