Other Parts Discussed in Thread: TPS23753A, TPS23753, PMP7355, TPS23754, PMP6812, PMP8803
Hello,
I am looking for a low cost TPS23753A reference design for 5V output using the Würth Elektronik transformer 749119350.
Regards,
Michael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Darwin,
we need a low-profile design with 10-13W power and below 9mm height. Maybe you do have a reference design with a transformer on a EFD15 or similar low profile core?
Best regards,
Michael
Hi Navin,
thank you so much for pointing me to your design change, based on the slvua27a. My only concern is that you are limited to 9W of output power by using only 2 of the 3 secondary windings of the 749119350.
We have based our design on the low cost reference design slvrb20.pdf, replacing the Coilcraft POE13P-50L with the Würth 749119350. Of course there is no synchronous but a single Schottky diode rectifier, so efficiency will not be as good as in your design.
Best regards,
Michael
Hi Darwin,
following your advice I have a functional TPS23753A low cost flyback design. Do you have a proposal for a TPS23754 low cost design?
I would need only 3W on the 3,3V output side but app. 20W on the 48-57V DC/DC input rail. Could I use the DC/DC flyback from the TPS23753A also on the TPS23754?
Regards,
Michael
Hi Ben,
sorry for not being clear. We have 2 boxes, one local and one remote, which are connected by a DC@48V 2-wire line. Usually the local box would feed 48V@0.6A to the remote box. The remote box has a bridge rectifier at the 2-wire input, in order to safeguard against wrong polarity of the 2-wire line. So the 2-wire line is polarity agnostic. In this case the local box provides the power output and the remote box the power input.
However, if there is no power at the local end available, we would like the option to reverse feed the local box from the remote box. In this case the power input and output are reversed and we have the task to go around the bridge rectifier for the reverse power direction. One idea was to use 2 hot-swap circuits and enable them for each direction.
Does this help? --Michael
Hi Michael,
Thanks for your update!
We don't have 12V and 3.3V reference design. But we can modify the schematic from PMP8752.
Change sendary MOSFET to diode, transformer,connect DT to VB,etc.
If you need any help, please contact us.
-Ben
Hi Ben,
I have 3 PoE reference designs with 12V output:
- SLVU314F (with components selected for 12V from the BOM)
- PMP6812
- PMP8803
The point is that component values differ a lot, and I am confused which of the above I should use. For example the feedback loop or the series resistor for current sensing are quite different in terms of resistor and capacitor values
Best regards,
Michael
Hi MIchael,
We have PMP4745 which is 12V@1A application.
You can refere to application note, SLVA305C, to modify the schematic and match your spec.
--Ben
If this post answered your question, please click Verify Answer.
Hi Ben,
I have done so. Would you be willing to take a look at the schematics in order to catch anything I might have overlooked?
Please note that the design is a "no electrolytics" one and uses only ceramics (X7Rs).
Best,
Michael
Hi Michael,
below are my suggestion.
1. C69 value should be 0.05uF to 0.1uF
2. What are your rated voltage of input cap? (C73, C74, C75, C76)
3. 80K ohm for R35 is enough.
4. Please check R34, R35, R44, R51 Size.
5. What is the function of D10?
-Ben
If this post answered your question, please click Verify Answer.
Ben Kuo said:Hi Michael,
below are my suggestion.
1. C69 value should be 0.05uF to 0.1uF
OK, thank you!
2. What are your rated voltage of input cap? (C73, C74, C75, C76)
They are all 100V: 100V_4u7_1812
3. 80K ohm for R35 is enough.
OK
4. Please check R34, R35, R44, R51 Size.
R_TF_20R_5_0805 |SMT 0805 5% 0,5W |R34,R51
R_MS_100K_1_0805 |SMD 100ppm 0,125W Cad=C |R35
R_MS_0R51_1_1206 |SMD 75ppm 0,250W Cad=M |R44
5. What is the function of D10?
I found D10 in one of the reference designs. I would presume the Zener acts as a safety device to keep the voltage on the APG Pin below 5.1 V.
-Ben
--Michael
If this post answered your question, please click Verify Answer.
Hi Michael,
There should be no issue with using 0.1uF. It is typical in most of our PD designs.
Hi Darwin,
iI am referring to the eval schematic of slvu304c.pdf:
Question: To what extend can I decrease the value of R2 (now: 6.49k) in order to make the LED D21 brighter?
Best regards,
Michael