This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We need to read the dfi file from dataflash of BQ27510-G3 chip.
Where we get the source code for this?
Please help.
Regards,
Anoop
Hello Aju,
You can use bqEVSW for bq27510-G3 and extract the DFI file from the gauge. On bqEVSW go to the bqEASY tab and manually navigate to step #3, Calibrate, where step 3F corresponds to reading the DFI from the device. Please ensure the device is unsealed and in full access to be able to extract the DFI file.
Thanks.
Hi,
Thanks for reply.
We need to read the dfi file from data flash of BQ27510-g3 chip from a microcontroller without using bqEVSW software.
For that , we need to implement c code by referring read data flash image flowchart from "Data Flash Programming and Calibrating bq27500 Gas Gauge(SLUA440)" document
Our query is that any sample C code availabe with ti to read back dfi file from the data flash of BQ27510-G3.If not ,can we refer above document to implement this logic?
We already flashed .dfi file size of 1025 bytes in the dataflash of BQ27510-g3 chip
We are trying to read this file from data flash and compare with the .dfi file of size 1025byte.
From the above documents,We understood that data flash has a size of 1548 bytes(0x06C0).So how we compare these files of different size.
Our motive is to ensure and crosscheck that dfi file is properly written in data flash.
Please help.
Regards,
Anoop
Hi Anoop,
The flashstream format is a text script with i2c commands that allow you to parse the data on the chip. There are checksums and compare commands that ensure the integrity of the data being parsed on the chip. Have you review the flash stream format document? See attached.
Hi,
Thanks for reply.Wil check that.
we see a difference in the ROM mode exit command in below documents
In document SLUA449F( Going to Production with the bq275xx), see 0x08 command to exit ROM mode
In document SLUA440(Data Flash Programming and Calibrating bq27500 Gas Gauge)see 0x0F command to exit ROM mode
Can you please clarify?
Hi,
We left the attempt to read entire dfi file because it need to put the chip in ROM mode.It may increase the error rate.
So is there any other mechanism to verify that proper dfi is written in the BQ27510G3 data flash?
If yes,please share the details.
Regards,
Anoop
Hi,
We sealed the BQ27510 chip.But we cannot unseal it.
Please find the steps that we done for sealing and unsealing
1.To seal the device,send 0x0020 to control register.And the device went to sealed mode.
2.To unseal the chip,we put 0x0414 and 3672 into the control register.But the device cannot unseal.And we cannot access to data flash areas after unseal.
What we can do to access the dataflash again?
Regards,
Anoop
Hi,
We do not use any key for sealing.
We just send 0x0020 to control register.
So How can we unseal the BQ27500 chip?
We already tried with 0x0414 and 0x3672 and swap the byte order also as you said
Please help.
Regards,
Anoop
Please use the guide in chapter 4.1 from the bq27510-G3 TRM instead of SLUA449F to access the data flash. You can use the block checksums to verify integrity.
Hi,
In BQ27510 chip,there is a command to know the chip in selaed or unsealed mode(SS bit in control status register)
Is there any similar command available in this chip to know the chip in ROM mode(Data flash access mode) or normal mode(battery monitoring mode)
Regards,
Anoop
Hi,
Thanks for reply..
For bq27510 chip,We are using battery monitor i2c address 0xAB for read operation and 0xAA for write operation(#define BMON_I2C_ADDRESS 0x55)
And using dataflash i2c address 0x17 for read operation and 0x16 for write operation(#define DFI_FLASH_I2C_ADDRESS 0x0b)
But we cannot understand how we get 0x16 and 0x44 device address.Please clarify.
Regards,
Anoop
Hi,
Ok.We can use 0x16 device address for access in ROM mode.
Which register in ROM mode we read and crosscheck to verify that we are in rom mode
Regards,
Anoop
For device address 0x16.
You can read register 0. If it ACKs then it is in ROM mode. You don't have to verify the actual content.