Hi Sir,
Can suggest me which function diagram is better?
Application LORA sensor box.pptx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
Can suggest me which function diagram is better?
Application LORA sensor box.pptx
Hi Nowal,
I prefer the solution on Page 2.
I'm not sure if the MCU can still work if input supply is 1.5V or lower. In consideration of stability and full usage of bettery, a boost is suggested for MCU power supply. Besides, a low noise power supply is also recommeded for a light sensor.
one thing noted is the current capability of TPS610981 if it supplys all the three load.
BR,
Gene