Hello.
My customers are looking for a modular product (ex:LMZ3xxxx etc) that can be used in the following specification .
Do you have the product information in the development ?
<specification>
・VIN:12V more
・VOUT:~4.5V(max)
・IOUT:20A
Want Answer Date:2016/6/24
Please tell me if any information even a little .
" Alone Yes or No"
Best Regards,
Masumi Sekiguchi