Hello again,
Reminder: We are currently using the TPS62160 in our designs for both 5V and 3.3V. You can find the schematics and layouts in a previous post here:
We've come across another strange issue with our 3.3V power supply on one of our boards.
When powered with a 12V power supply, the 3.3V DC/DC fails to output the correct voltage. Instead i measured 5.50V. Furthermore, if i reduce the input voltage, the output voltage also reduces. There seems to be a linear relation between Input->output voltage. Some measurements:
Vin -> Vout
12V -> 5.5V
10V ->5.25
8V -> 4.4V
6.5V -> 3.38V
6V down to 3.3V -> 3.3V
What is even more surprising, is that once i reach ~6V, the DC/DC Starts to switch, and the output voltage is the correct. Furthermore, in the "operating region" (6V to 3.3V), the switching signal, output voltage, feedback voltage, all look correct.
Once the voltage was at the correct 3.3V, i could flash the MCU (i was supprised to see that it still works..) on our board. Doing so increases the load current by about 40mA. after doing so, the DC/DC would work for the entire input voltage range 12.5V to 3.3V.
I'm not sure what to make of this. I'm assuming that the DC/DC is damaged, but cannot understand why or how.
Any help would be most appreciated!
Thanks,
Alex