Hi, team,
Customer is developing an quasi-resonant fly-back power application using UCC24630.
UCC24630 was changed from UCC24636, because of same high current issue, about one month ago.
The high current of over 10 A still occurs irregularly at the red elliptic circle timing of the attached waveform in the power up period using UCC24630.
Waveforms and schematics are attached.
VIN=170 Vac, Vout=5 V, Iout=16 A,
Transformer : 420 uH, Np=31 T, Ns=2 T.
What kinds of problems are considered?
How can we get rid of this high over current issue?