Hi all
Would you mind if we ask LMR23625(LMR2625CF)?
We'd like to realize the following spec using LMR23625(LMR2625CF).
-Vin=12V, Vout=-16V, Iout=1.0A, L=4.7uH, F=2.1MHz
-D=|Vout|/Vin+|Vout|
-IOUT(MAX) = (ICLMIN – (VIN x D)/(2 x F x L)) x (1 - D)
Iout(MAX)=1.03A
We guess that it is possible.
Is our recognition correct?
Kind regards,
Hirotaka Matsumoto