Hello,
I'm trying to get the best accuracy for current sense of BQ34Z100-G1.
My pack will see 1A maximum current (when charging) and should have discharge current in the range of 10-200mA.
So It seems that the best Rsns would be 100mOhms (max current is 1.25A=>OK, and Iwake=12.5mA=> I'd preferred less than 10mA but it should be OK).
But it's impossible to program it with BQstudio (OK for CC Delta, but CC gain return (Value is beyond minimum value defined for parameter, even with 50mOmh).
Is it possible to have more than 40mOhms?
Regards,
Hubert