This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: LM5116 Schematic Review

Part Number: LM5116

Hi,

Any one can review my attached schematic, which is based on LM5116. below are the Inputs to review the schematic.

Part No: LM5116MH/NOPB

Vin (nominal)=10V

Vout =3.3V

Iout= 3.5A

SW frequency: App. 1MHZ.

Please feel free to ask for any other inputs.

it would be great if any one can go through the MOSFET Selection parameters and review the design. (When select LOW side FET as IRF8714, it was not taking in web-bench, i don't it is tools error or design error ).

Thanks in Advance.

Ranganadh

LM5116.pdf