This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have a board with cell balance circuit similar to that shown in the specsheet/appnotes and am questioning the appropriate register values for using the stand-alone cell balancing.
Specifically, the values in OV_CFG (0x06) for the OV level.
My understanding is that in this case, OV2-0 are used as the cell voltage which triggers the balancing algorithm.
If this is the case, the default (0x00) for this field would be the proper value when balancing, correct?
I observe cell voltages exceeding the register value during the balance process, so the process should start as early as possible, correct?
I have studied slus844b and slua463, but any other resource would be helpful.
Thanks