[ LM3435 ] SVDD Supply Range and Power Sequencing
Dear forum member,
Could you help to check the supply voltage range of SVDD of LM3435?
I can find the specification for VIN, however, no clear description for SVDD range.
The information, I can find out from datasheet is below.
However, different information can be seen on the following post from Mr. Issac.
"Yes, it is ok to connect SVDD to VIN (as long as it is above 2.5 V)."
LM3435 / unused pin, control freq
e2e.ti.com/.../552806
Can you clarify the valid SVDD supply range?
Also, is there are the requirements and/or restrictions on power supply sequence between VIN and SVDD?
Thank you for your support in advance.
Regards,
Ken