I need a LED driver that can power a sting of LEDs which will illuminate an area that can range from pitch black to well lit (LEDs off). The device will be battery powered, but due to the limitations of the camera module the control unit and camera module will have to use the same power source, that unfortunately will not also be able to power the LED circuit. I was wondering if there were any drivers that can take input from the control unit that is a separate circuit from that which powers the LED driver and array (which would simplify the design quite a bit).