This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team:
My customer using TPS56628 in their project, but they find the TPS56628's output ripple is about 100mV when the output voltage is 5V.
Could you help me to verify whether this is the best ripple performnace of our part? Any way to improve it? Thanks.
Hi, Derek,
could you show us snapshot of the output ripple waveform?
how do you test the output ripple?
Best Regards,
Nick
Hi Yuchang:
We have limited the bandwidth to 20MHz. The output inductor is 1uH and 50uF total. But we try different inductor and capacitor. No much improvment.
We have verify the EVM, the ripple is also around 100mV(Vpp). Could you please optimize the EVM to see what's best ripple at the light load? Thanks.
Derek,
description from datasheet page 7: (red words)
Auto-Skip Eco-mode™ Control
The TPS56628 is designed with Auto-Skip Eco-mode™ to increase light load efficiency. As the output current
decreases from heavy load condition, the inductor current is also reduced and eventually comes to a point where
its rippled valley touches zero level, which is the boundary between continuous conduction and discontinuous
conduction modes. The rectifying MOSFET is turned off when its zero inductor current is detected. As the load
current further decreases the converters runs in discontinuous conduction mode. The on-time is kept almost the
same as it was in the continuous conduction mode
so, if the VIN and Vout is fixed, so the on-time is fixed too.
to decrease the ripple, two approach: increase inductor value; increase Cout value. But for this device, inductor and Cout has limited according to the Vout, refer datasheet page 13, table 1.
Jason Wang