Customer wants to design a 5V 7.5W application referring the EVM.
Is it enough change that only current sense resistance is changed from 2.15 ohm to 1.56 ohm, using the same transformer with Lp=1.5 mH and turns ratio of 15.42:1?
Is the switching frequency automatically adjusted by the internal CC regulation?
Do CV and CC output control get any problems?