If there match solution for 2kW~3kW buck PFC on TI device, please let me know.
【Additional information】
・Input: 440Vac
・Output: 270V / 2kW~3kW
・Customer is aiming at PF:0.95
・60Hz
Best regards,
Satoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If there match solution for 2kW~3kW buck PFC on TI device, please let me know.
【Additional information】
・Input: 440Vac
・Output: 270V / 2kW~3kW
・Customer is aiming at PF:0.95
・60Hz
Best regards,
Satoshi
Satoshi,
From another thread:
"The only Buck PFC controller in the TI portfolio is the UCC29910A. It was developed to produce a 84V output from universal line input of 85V to 264V and it is not possible to change the input/output RATIO. If you use this device you will have to scale the output accordingly and I estimate that Vo would be about 150V. This could then be fed into the LLC second stage.
Be aware that the BUCK PFC works well but has the disadvantage of being more susceptible to input surges (lightening strikes) than the more usual Flyback.
A 'normal' boost PFC will have an output voltage above 650V if you wish to operate it at 460Vac in."
The datasheet says a power factor of >0.9 so I'll have to wait for someone else to comment about reaching 0.95.
-Sam
Hello Satoshi
The Buck PFC can get 0.95 PF but not at low line where the 'dead time' - the time where the instantaneous input voltage is less then the output voltage - is large. So, it depends on the input voltage range you are working with.
Take a look at the article at https://www.ti.com/seclit/ml/slup264/slup264.pdf for more details.
Regards
Colin